Renesas Electronics
Error messages are output.
The output example of the error information is shown below.
*** Error Information ***
** E0562310 Undefined external symbol "_func_02" referenced in "sample.obj" (1)
Number
Description
(1)
Error message