3.4.3 Error information

Messages for errors or warnings are output.

The output example of the error information is shown below.

*** Error Information ***
 
** E0561200 Backed up file "sample1.lib" into "usrlib.lbk"      (1)

Number

Description

(1)

Message

The message is output.