Renesas Electronics
HIGHW
Returns the high-order 16-bit value of a term.
[Function]
[Application example]
movea HIGHW(0x12345678), R0, r10 ; (1)
(1)
By executing a movea instruction, this operator returns the high-order 16-bit value "0x1234" of the expression "0x12345678". Therefore, (1) in the above example can also be described as: movea 0x1234, R0, r10.