.stack


Defines the stack amount of consumption for a symbol.

[Syntax]

Symbol field
Mnemonic field
Operand field
Comment field
 
.stack
symble-name=value
[; comment]

[Function]

-

The .stack directive is compiler debugging information.

[Description]

-

This defines the stack amount of consumption for a symbol.

-

The stack amount of consumption for a symbol can only be defined once, and subsequent definitions are ignored.

-

The stack amount of consumption can only be defined as a 4-byte range of 0x0 to 0xFFFFFFFC. If a different value is specified, then the definition is ignored.

-

This is the function information of the C source program that the compiler outputs.