Symbol field |
Mnemonic field |
Operand field |
Comment field |
[label:] |
.db |
expression[, ... ] |
[; comment] |
[label:] |
.db |
"Character string constants" |
[; comment] |
The .db directive tells the assembler to initialize a memory area in byte units with the initial value(s) specified in the operand field. |
The value of an expression must be 1-byte data. Therefore, the value of the operand must be in the range of 0x0 to 0xFF. If the value exceeds 1 byte, the assembler will use only lower 1 byte of the value as valid data.
If the first operand is surrounded by corresponding double quotes ("), then it is assumed to be a string constant.
If a character string constants is described as the operand, an area of appropriate size will be reserved for each character in the string.
As an initial value, an expression that includes a relocatable symbol or external reference symbol may be described. |
If the relocation attribute of the section containing the .db directive is "BSS", then an error is output because initial values cannot be specified. |
.dseg data MASSAG: .db "ABCDEF" ; (1) DATA1: .db 0xA, 0xB, 0xC ; (2) DATA3: .db "AB" + 1 ; (3) <- Error |