This directive skips the repetitive assembly of the .irp and .rept directives enclosing this directive at the innermost position.
[Syntax]
Symbol field 
 | 
Mnemonic field 
 | 
Operand field 
 | 
Comment field 
 | 
[label:] 
 | 
.exitm 
 | 
  
 | 
[; comment] 
 | 
 
[Function]
-  | This directive skips the repetitive assembly of the .irp and .rept directives enclosing this directive at the innermost position.  | 
 
[Description]
-  | If this directive is not enclosed by .irp and .rept directives, the assembler outputs the message then stops assembling.  |