ENDIF


End of control range.

[Syntax]

[]$[]ENDIF[]absolute-expression[][;comment]

[Function]

Indicates the end of the control range of a conditional assembly control instruction.

[Use]

-

With these conditional assembly control instructions, source statements subject to assembly can be changed without major modifications to the source program.

-

If a statement for debugging that becomes necessary only during the program development is described in a source program, whether or not the debugging statement should be assembled (translated into machine language) can be specified by setting switches for conditional assembly.