A macro is described by registering a pattern with a set sequence and by using this pattern. A macro is defined by the user. A macro is defined as follows. The macro body is enclosed by ".macro" and ".endm".
PUSHMAC .macro REG ;The following two statements constitute the macro body. add -4, sp st.w REG, 0x0[sp] .endm  | 
If the following description is made after the above definition has been made, the macro is replaced by a code that "stores r19 in the stack".
In other words, the macro is expanded into the following codes.