Read character from stream (same as fgetc)
Remark  | These functions are not supported by the debugging functions which CS+ provides.  | 
 
[Classification]
Standard library
[Syntax]
#include <stdio.h>
int getc(FILE *stream);
[Return value]
The input character is returned.
Error return does not occur.
[Description]
This function inputs one character from the input stream pointed to by stream.  Only the standard input/output stdin can be specified for stream.