lldiv_t lldiv(long long n, long long d);
The structure storing the result of the division is returned.
This function is used to divide a value of long long type.
This function calculates the quotient and remainder resulting from dividing numerator n by denominator d, and stores these two integers as the members of the following structure div_t.
quot the quotient, and rem is the remainder. If d is not zero, and if "r = div(n, d);", n is a value equal to
"r.rem + d * r.quot".
If d is zero, the resultant quot member has a sign the same as n and has the maximum size that can be expressed. The rem member is 0.
The operation is undefined when the -Xansi option is specified.