7.4.12 Peripheral device initialization function

The peripheral device initialization function is as follows.

Table 7.14

Peripheral Device Initialization Function

Function/Macro Name

Outline

hdwinit

Initialization of peripheral devices immediately after the CPU reset