11.2  V850E3v5 G3K Core Specification for Assembler (-Xcpu=g3k Option)
 
The following instruction sets cannot be specified.
-  | Hardware multithreading feature instructions  | 
 
-  | Virtualization support feature instructions  | 
 
-  | MMU control instructions  | 
 
-  | Floating-point operation instructions  | 
 
 
The above instruction sets cause assemble errors when the V850E3v5 G3K core is specified. If any of them is specified, the assembler outputs the following message.
| 
 
E0550269 : Illegal mnemonic(cannot use this mnemonic ins RH850 "G3K" core). 
 |