A.1.1.1 GP relative access
This generates code to access variables using one instruction by placing variables in sections that can be accessed via the global pointer (GP) and an ld/st instruction.
Use a #pragma section directive when defining or accessing variables, and specify either gp_disp16 or gp_disp23 as the attribute strings.
#pragma section attribute-strings
variable-declaration/definition
#pragma section default
|
Example 1. | Accessing via a GP-relative 4-byte load/store instruction |
#pragma section gp_disp16
int a = 1; /*allocated to .sdata section*/
int b; /*allocated to .sbss section*/
#pragma section default
|
Example 2. | Accessing via a GP-relative 6-byte load/store instruction |
#pragma section gp_disp23
int a = 1; /*allocated to .sdata23 section*/
int b; /*allocated to .sbss23 section*/
#pragma section default
|