| 
 | 
 | 
 | 
 | 
| 
 
C source file 
 | 
 
.c 
 | 
 | 
 
Source file described in C language 
This is created by the user. 
 | 
| 
 
Preprocessed file 
 | 
 
.iNote 1 
 | 
 | 
 
Text file which the execution result of preprocess processing for the input file is output 
This file is output when the -P option is specified. 
 | 
| 
 
Assembly source file 
 | 
 
.asmNote 1 
 | 
 | 
 
Assembly language file generated from C source file by compilation 
This file is output when the -S option is specified. 
 | 
| 
 
.asm 
.s 
 | 
 | 
 
Source file described in assembly language 
This is created by the user. 
 | 
| 
 
Header file 
 | 
 
free 
 | 
 | 
 
File referred by source files 
This file is described in C language or assembly language. 
This is created by the user. 
The extension is free, but the following is recommended. 
-  | $include control instruction: .inc  |  
  
 | 
| 
 
Object file 
 | 
 
.objNote 1 
 | 
 | 
 
ELF-format file including machine-language information, relocation information relating to machine-language allocation addresses, and symbol information 
 | 
| 
 
Assemble list fileNote 2 
 | 
 
.prnNote 1 
 | 
 | 
 
List file which has information from the assemble result 
This file is output when the -asmopt=-prn_path option is specified. 
 | 
| 
 
Library file 
 | 
 
.libNote 1 
 | 
 | 
 
ELF-format file in which two or more object files are included 
This file is output when the -lnkopt=-form=library option is specified. 
 | 
| 
 
Load module file 
 | 
 
.absNote 1 
 | 
 | 
 
ELF-format file of the object code of the link result 
This is the input file when a hex file is output. 
This file is output when the -lnkopt=-form=absolute option is specified. 
If you specify the -lnkopt option but not the -form option, the command assumes that the above option has been specified. 
 | 
| 
 
Relocatable file 
 | 
 
.relNote 1 
 | 
 | 
 
Relocatable object file 
This file is output when the -lnkopt=-form=relocate option is specified. 
 | 
| 
 
Intel HEX fileNote 2 
 | 
 
.hexNote 1 
 | 
 | 
 
Load module file converted into the Intel HEX format 
This file is output when the -lnkopt=-form=hexadecimal option is specified. 
 | 
| 
 
Motorola S-record fileNote 2 
 | 
 
.motNote 1 
 | 
 | 
 
Load module file converted into the Motorola S-record 
This file is output when the -lnkopt=-form=stype option is specified. 
 | 
| 
 
Binary file 
 | 
 
.binNote 1 
 | 
 | 
 
Load module file converted into the binary format 
This file is output when the -lnkopt=-form=binary option is specified. 
 | 
| 
 
Symbol address file 
 | 
 
.fsy 
 | 
 | 
 
Assembly source file where external defined symbols are described in assembler directives 
This file is output when the -lnkopt=-fsymbol option is specified. 
 | 
| 
 
Link map fileNote 2 
 | 
 
.mapNote 1 
 | 
 | 
 
List file which has information from the link result 
This file is output when the -lnkopt=-list option is specified. 
 | 
| 
 
Library list fileNote 2 
 | 
 
.lbpNote 1 
 | 
 | 
 
List file which has information from the library creation result 
This file is output when the -lnkopt=-list option is specified. 
 | 
| 
 
Stack information file 
 | 
 
.sni 
 | 
 | 
 
List file which has information of the stack capacity 
This file is output when the -lnkopt=-stack option is specified. 
 | 
| 
 
Variable/function  
information file 
 | 
 
.hNote 1 
 | 
 | 
 
File containing declarations of the saddr variable or callt function 
This file is output when the -lnkopt=-vfinfo option is specified. 
 | 
| 
 
Static analysis information file 
 | 
 
free 
 | 
 | 
 
File which has information from the static analysis result 
The extension is free, but ".cref" is recommended. 
This file is output when the -cref option is specified. 
 | 
| 
 
Error message file 
 | 
 
free 
 | 
 | 
 
File which contains error messages 
The extension is free, but ".err" is recommended. 
This file is output when the -error_file option is specified. 
 | 
| 
 
Subcommand file 
 | 
 
free 
 | 
 | 
 
File which contains the parameters of the execution program 
This is created by the user. 
 |