This option outputs the list file.
[Specification format]
- | Interpretation when omitted |
None
[Detailed description]
- | This option outputs list file file. |
- | An error will occur if the specification of the file name is omitted. |
|
|
|
|
|
-form=library option or -extract option
|
Library list file
|
Output file nameNote.lbp
|
|
Other than above
|
Link map file
|
Output file nameNote.map
|
Note | If there are two or more output files, this is the first input file name. |
[Example of use]
- | To output the link map file to file.map, describe as: |
>rlink a.obj b.obj -list=file.map
|