|
-SYmbol_forbid [V1.02 or later]
|
This option disables optimization regarding deletion of unreferenced symbols.
[Specification format]
-SYmbol_forbid=symbol-name[,symbol-name]...
|
- | Interpretation when omitted |
Optimization regarding deletion of unreferenced symbols is not disabled.
[Detailed description]
- | This option disables optimization regarding deletion of unreferenced symbols. |
[Example of use]
- | To disable optimization of the _func symbol, describe as: |
>rlink a.obj b.obj optimize symbol_forbid=_func
|
[Remark]
This option is ignored if optimization is not applied at linkage.