3.2.5 Link map information

Start/end addresses, size, and type of each section are output in the order of address.

The output example of the link map information is shown below.

*** Mapping List ***
 
(1)                                (2)        (3)         (4)     (5)
SECTION                            START      END         SIZE    ALIGN
 
.textf
                                  00000100  0000013b        3c    1
.data
                                  000f0400  000f0403         4    2
.bss
                                  000f0404  000f0407         8    2

Number

Description

(1)

Section name

The name of the section is output.

(2)

Start address

The start address is output.

This is expressed in a hexadecimal number.

(3)

End address

The end address is output.

This is expressed in a hexadecimal number.

(4)

Section size

The section size is output (byte).

This is expressed in a hexadecimal number.

(5)

Section alignment size

The section alignment size is output.