Add #include directive to the C source files to include variable/function information file, and then compile the files. |
Specifying -preinclude option is another way to include the information file. |
Variable/function information file can be edited manually. |