Initialization of 2-byte area.
The value of an expression must be 2-byte data. Therefore, the value of the operand must be in the range of 0x0000 to 0xFFFF. If the value exceeds 2-byte, the assembler will use only lower 2-byte value as valid 2-byte data.
An expression that includes a relocatable symbol or external reference name may be described.
If the relocation attribute of the section containing the .DB2 directive is "BSS", then an error is output because initial values cannot be specified. |