Control based on absolute expression (assembly performed when the value is false).
[Syntax]
[]$[]ELSEIFNabsolute-expression[][;comment]
|
[Function]
- | If the absolute expression specified by the operand is evaluated as being true ( 0). |
Skips to the ELSEIF, ELSEIFN, ELSE, or ENDIF control instruction corresponding to this control instruction.
- | If the absolute expression is evaluated as being false (= 0). |
(a) | If this control instruction and the corresponding ELSEIF, ELSEIFN, or ELSE control instruction exist, assembles the block enclosed within this control instruction and the corresponding control instruction. |
(b) | If none of the corresponding control instruction detailed above exist, assembles the block enclosed within this control instruction and the corresponding ENDIF control instruction. |