Defines a name having an absolute-expression value.
Defines a name having a absolute-expression value specified by the operand field.
You can use this directive to define names for numerical data that can be used instead of the actual numbers in the operands of machine-language instructions and directives in source code. |
We recommend defining frequently used numerical values as names. Even if a given value in the source program is to be changed, you will only need to change the value corresponding to the name. |
The name generated by the .SET directive cannot be externally defined by the .PUBLIC directive. |
The operand value is in accordance with "(a) Absolute expression". An illegal value will lead to an error. |
A value between 0x00000000 and 0xFFFFFFFF can be specified as an absolute expression in the operand field. |
This directive differs from the .EQU directive in that a symbol with a bit position specification cannot be defined. |
Operators that generate a relocatable term as a result of calculation are not allowed in the operand field. |
To specify a constant expression.