11.2.3 Options necessary at assembling the startup file
When startup is directly assembled without intervening the compiler driver, specify the following options.
-define=__RENESAS_VERSION__=0x01000000 ; When CC-RL V1.00 is used
-define=__RENESAS_VERSION__=0x01010000 ; When CC-RL V1.01 is used