11.3.7 An option depending on the order of specification of options
Option "-no_warning" has no effect if the order of specification of options is inappropriate.
Example | "-no_warning" has no effect in the following case.
-define=xxxx -undefine=xxxx -no_warning=50649
|
To suppress a warning message, perform either of the followings.
- | When the assember is invoked via the compile driver, |
- | specify compile option "-no_warning_num=50649", or |
- | specify "-asmopt=-no_warning=50649" before other options. |
- | When the assembler is invoked directly, |
- | specify "-no_warning" before the other options. |
Example | "-no_warning" has an effect in the following case.
-no_warning=50649 -define=xxxx -undefine=xxxx
|