Renesas Electronics
top
Compiler
COMPILER LANGUAGE SPECIFICATIONS
Basic Language Specifications
Static variable initialization
4.1.8 Static variable initialization
This section explains the static variable initialization.
Previous Topic
Allocation conditions for data and function
Next Topic
Initialization by address calculation
Table of Contents
Unspecified behavior
Undefined behavior
Processing system dependent items
C99 language function
Option to process in strict accordance with ANSI standard
Internal representation and value area of data
Allocation conditions for data and function
Static variable initialization
Initialization by address calculation
Casting far address to near address and then converting to far address