|
Inline expansion of function (#pragma inline, #pragma noinline) |
This notifies the compiler of an inline function.
#pragma noinline declares a function whose inline expansion is to be stopped when the -Oinline_level option is used. |
If both #pragma inline and #pragma noinline are specified for the same function within a single translation unit, an error will occur. |
The #pragma inline directive should be written before the definition of the target function within the translation unit that includes the function definition. |
#pragma inline has the same function as keyword __inline. For details of inline expansion, see "Specifying inline function (__inline)". |