|  |  |  | 
| __DI | 
Outputs a DI instruction. | void __DI(void); | 
| __EI | 
Outputs a EI instruction. | void __EI(void); | 
| __halt | 
Outputs a HALT instruction. | void __halt(void); | 
| __stop | 
Outputs a STOP instruction. | void __stop(void); | 
| __brk | 
Outputs a BRK instruction. | void __brk(void); | 
| __nop | 
Outputs a NOP instruction. | void __nop(void); | 
| __rolb | 
Rotates x to the left y times assuming that x has a size of eight bits.  
Operation is undefined for the case where the rotation count is greater than the size of the value. 
If the rotation count may be greater than the size, mask the count to not exceed the size. | unsigned char   x, y; unsigned char   __rolb(x, y); | 
| __rorb | 
Rotates x to the right y times assuming that x has a size of eight bits.  
Operation is undefined for the case where the rotation count is greater than the size of the value. 
If the rotation count may be greater than the size, mask the count to not exceed the size. | unsigned char   x, y; unsigned char   __rorb(x, y); | 
| __rolw | 
Rotates x to the left y times assuming that x has a size of 16 bits.  
Operation is undefined for the case where the rotation count is greater than the size of the value. 
If the rotation count may be greater than the size, mask the count to not exceed the size. | unsigned int    x; unsigned char   y; unsigned int    __rolw(x, y); | 
| __rorw | 
Rotates x to the right y times assuming that x has a size of 16 bits.  
Operation is undefined for the case where the rotation count is greater than the size of the value. 
If the rotation count may be greater than the size, mask the count to not exceed the size. | unsigned int    x; unsigned char   y; unsigned int    __rorw(x, y); | 
| __mulu | 
Executes 8-bit unsigned multiplication between x and y and returns a 16-bit result. | unsigned char   x, y; unsigned int    __mulu(x, y); | 
| __mului | 
Executes 16-bit unsigned multiplication between x and y and returns a 32-bit result. | unsigned int    x, y; unsigned long   __mului(x, y); | 
| __mulsi | 
Executes 16-bit signed multiplication between x and y and returns a 32-bit result. | signed int      x, y; signed long     __mulsi(x, y); | 
| __mulul | 
Executes 32-bit unsigned multiplication between x and y and returns a 64-bit result. | unsigned long   x, y; unsigned long long  __mulul(x, y); | 
| __mulsl | 
Executes 32-bit signed multiplication between x and y and returns a 64-bit result. | signed long     x, y; signed long long    __mulsl(x, y); | 
| __divui | 
Executes unsigned division between x and y and returns a 16-bit result. 
When divisor y is 0, 0xFFFF is returned. | unsigned int    x; unsigned char   y; unsigned int    __divui(x, y); | 
| __divul | 
Executes unsigned division between x and y and returns a 32-bit result. 
When divisor y is 0, 0xFFFFFFFF is returned. | unsigned long   x; unsigned int    y; unsigned long   __divul(x, y); | 
| __remui | 
Executes unsigned remainder operation between x and y and returns a 8-bit result. 
When divisor y is 0, the lower-order 8 bits of dividend x are returned. | unsigned int    x; unsigned char   y; unsigned char   __remui(x, y); | 
| __remul | 
Executes unsigned remainder operation between x and y and returns a 16-bit result. 
When divisor y is 0, the lower-order 16 bits of dividend x are returned. | unsigned long   x; unsigned int    y; unsigned int    __remul(x, y); | 
| __macui | 
Executes unsigned multiply-accumulate operation (unsigned long) x * (unsigned long) y + z, and returns a 32-bit result. | unsigned int    x, y; unsigned long   z; unsigned long   __macui(x, y, z); | 
| __macsi | 
Executes unsigned multiply-accumulate operation (signed long) x * (signed long) y + z, and returns a 32-bit result. | signed int      x, y; signed long     z; signed long     __macsi(x, y, z); | 
| __get_psw | 
Returns the contents of PSW. | unsigned char   __get_psw(void); | 
| __set_psw | 
Sets x to PSW. | unsigned char   x; void            __set_psw(x); | 
| __set1 | 
The set1 instruction is used to set bit y of the address indicated by x to 1. 
Only a constant from 0 to 7 can be specified for bit y and a compile error will occur when any other value is specified. | unsigned char   __near *x; unsigned char   y; void            __set1(x, y); | 
| __clr1 | 
The clr1 instruction is used to clear bit y of the address indicated by x to 0. 
Only a constant from 0 to 7 can be specified for bit y and a compile error will occur when any other value is specified. | unsigned char   __near *x; unsigned char   y; void            __clr1(x, y); | 
| __not1 | 
The not1 instruction (xor instruction for the saddr area) is used to invert bit y of the address indicated by x. 
Only a constant from 0 to 7 can be specified for bit y and a compile error will occur when any other value is specified. | unsigned char   __near *x; unsigned char   y; void            __not1(x, y); |