Perform division of int type to obtain the quotient and remainder
div_t __far div(int n, int d);
The structure storing the result of the division is returned. When divided by 0, -1 is set to quotient quot and n is set to remainder rem.
This function is used to divide a value of int type
This function calculates the quotient (quot) and remainder (rem) resulting from dividing numerator n by denominator d, and stores these two integers as the members of the following structure div_t.
When the value cannot be divided, the quotient of the result becomes an integer that is closest to the algebraical quotient but has a smaller absolute value.