7.1 Supplied Libraries

The CC-RL provides the following libraries.

Table 7.1

Supplied Libraries

Supplied Libraries

Library Name

Outline

Standard library

 

[V1.03 or later]

(except for calloc, free, malloc, and realloc)

rl78nm4s.lib

For an 8-bit or 16-bit CPU without extended instructions and arithmetic units

rl78cm4s.lib

For a 16-bit CPU using division/multiplication and multiply-accumulate units

rl78em4s.lib

rl78em8s.lib

For a 16-bit CPU using division/multiplication extended instructions

[V1.03 or later]

Standard library

(calloc, free, malloc, realloc)

malloc_n.lib

malloc library for normal usage

malloc_s.lib

malloc library for security facility

[Professional Edition only]

Runtime library

rl78nm4r.lib

For an 8-bit or 16-bit CPU without extended instructions and arithmetic units

rl78cm4r.lib

For a 16-bit CPU using division/multiplication and multiply-accumulate units

rl78em4r.lib

rl78em8r.lib

For a 16-bit CPU using division/multiplication extended instructions

Startup routine

cstart.asm

Startup routine

 

In order to pass the far pointer to a standard library function that has a variable pointer as a parameter, the user has to call the function for the far variable pointer whose function name starts with "_COM_". Note that when the -far_rom option is specified, the function macros of the header file are valid and the function for the far variable pointer is automatically called.