There are two variants of this license - the Professional Edition and the Standard Edition. The usable options are limited in the Standard Edition.
For the usable options in the Professional Edition, see "Table 2.2 Compile Options" or the description for each option.
The functions of the Professional Edition can be used with the free evaluation license within the evaluation period.
There are two license types, and the license is confirmed with the following priority.
Floating license  | 
When none of the following conditions are met at linkage, the license is regarded as a free evaluation one and the total size of linked objects is restricted.
The evaluation period of 60 days has not passed since the first time the optimizing linker was invoked.  | 
The size limitation specifies that for a section whose section type is PROGBITS and whose section attribute is allocate, the total size of the section should be up to 64 Kbytes. When the size exceeds 64 Kbytes, an error will occur.
The version sign of the optimizing linker is W when operating as a free evaluation version and is V when operating as a paid version.