|
|
|
|
|
|
C source program file
|
.c
|
Input
|
A source file written in C99 language.
This file is created by the user.
|
|
C++ source program file
|
.cpp, .cp, and .cc
|
Input
|
A source file written in C++ language.
This file is created by the user.
|
|
Include file
|
Optional
|
Input
|
A file referenced by the source file and written in C, C99, C++, or assembly language.
This file is created by the user.
|
|
Preprocessor expansion file for the C program
|
.p
|
Output
|
A file output as a result of preprocessing applied to an input C-language or the C99-language source program.
An ASCII image file.
This is output when the -output=prep option is specified.
|
|
Preprocessor expansion file for the C++ program
|
.pp
|
Output
|
A file output as a result of preprocessing applied to an input C++-language source program.
An ASCII image file.
This is output when the -output=prep option is specified.
|
|
Assembly-source program file
|
.src
|
Output
|
An assembly-language file generated from a C, C99, or C++ source file through compilation.
|
|
.src
|
Input
|
A source file written in assembly language.
|
|
List file for the assembly program
|
.lst
|
Output
|
A list file containing the assembly result information.
This is output when the -listfile option is specified.
The output contents are selected with the -show option.
|
|
Relocatable object program file
|
.obj
|
Output
|
An ELF-format file that contains the machine-language information, the relocation information about the allocation addresses of machine-language instructions, and symbol information.
|
|
Absolute load module file
|
.abs
|
Output
|
An ELF-format file for the object code generated as a result of linkage.
This is an input file when a hex file is output.
|
|
Linkage list file
|
.map
|
Output
|
A list file containing the linkage result information.
This is output when the -list option is specified.
The output contents are selected with the -show option.
|
|
Library file
|
.lib
|
Output
|
A file where multiple object module files are registered.
|
|
Library list file
|
.lbp
|
Output
|
A list file containing the result information of generation of the library.
This is output when the -list option is specified.
The output contents are selected with the -show option.
|
|
Library backup file
|
.lbk
|
Output
|
File type for saving the contents of original library files before they are overwritten by the library generator.
|
|
Hex file (Motorola S-format file)
|
.mot
|
Output
|
A Motorola S-format file in the hex format converted from the load module file.
|
|
Hex file (Intel (expansion) hex format file)
|
.hex
|
Output
|
An Intel (expansion) file in the hex format converted from the load module file.
|
|
Hex file (binary format file)
|
.bin
|
Output
|
A binary file in the hex format converted from the load module file.
|
|
Stack information file
|
.sni
|
Output
|
A stack information file.
This is output when the -stack option is specified.
|
|
Debugging information file
|
.dbg
|
Output
|
A debugging information file.
This is output when the -sdebug option is specified.
|
|
Object file including a definition specified with a file having extension td
|
.rti
|
Output
|
An object file including a definition specified with a file having extension td.
|
|
Calling information file
|
.cal
|
Output
|
A calling information file.
This is output by CallWalker.
|
|
External symbol assignment information file
|
.bls
|
Output
|
An external symbol assignment information file.
This is output at linkage when the -map option is specified.
|
|
.bls
|
Input
|
An external symbol assignment information file.
This is specified as an input file for the -map option at compilation.
|
|
Jump table file (assembly language)
|
.jmp
|
Output
|
An assembler source file for the jump table that branches the external definition symbol.
This is output when the -jump_entries_for_pic option is specified.
|
|
Symbol address file (assembly language)
|
.fsy
|
Output
|
An assembler source file that describes the external definition symbol in an assembler directive.
This is output when the -fsymbol option is specified.
|
|
C++ language function support file
|
.td, .ti, .pi, and .ii
|
Output
|
An information file that supports the C++ language function.
|