-listfile


< Assembler Command Options / List Options >

[Format]

-listfile[=<file name>]

 

-

[Default]

If this option is not specified, no assemble list file is output.

[Description]

-

When the listfile option is specified, an assemble list file is output. The name of the file can also be specified.

-

<file name> should be specified according to the rules described in the Naming Files section.

-

If <file name> is not specified in the listfile option, the source file name with the extension replaced with .lst is used as the source list file name.