-isa


< Assembler Command Options / Microcontroller Options >

[Format]

-isa={ rxv1 | rxv2 }

 

-

[Default]

The default for this option is determined based on the environment variable ISA_RX.

[Description]

-

This option is used to select an instruction-set architecture (RXv1 or RXv2) for use in generating instruction codes.

-

When -isa=rxv1 is specified, an instruction code for the RXv1 instruction-set architecture is generated.

-

When -isa=rxv2 is specified, an instruction code for the RXv2 instruction-set architecture is generated.

[Remarks]

-

When neither the -nofpu nor -fpu option has been selected, specifying the -isa option automatically selects the
-fpu option.

-

Omitting the -isa option will lead to an error if neither the -cpu option nor one of the environment variables (CPU_RX or ISA_RX) is specified.

-

The -isa and -cpu options cannot be specified at the same time.