-samesize


< Optimizing Linkage Editor (rlink) Options / Optimize Options >

[Format]

-samesize = <size>

 

-

[Default]

When this option is omitted, the default is samesize=1E.

[Description]

-

Specifies the minimum code size for the optimization with the same-code unification (optimize=same_code). Specify a hexadecimal value from 8 to 7FFF.

[Remarks]

-

When optimize=same_code is not specified, this option is unavailable.