3.2.3 Error Information

Error messages are output. The following figure shows an example of error information output.

*** Error Information ***
** E0562310 (E) Undefined external symbol "strcmp" referred to in "test.obj"  (1)

Item Number

Description

(1)

Outputs an error message.

Note

As the number for the alignment of code sections whose address is determined after linkage, when big endian is selected, a multiple of 4 is indicated regardless of the actual number for alignment at the time of compiling and assembling.