3.3.1 Structure of Library List

Table 3.4 shows the structure and contents of the library list.

Table 3.3

Structure and Contents of Library List

No

Output Information

Contents

SuboptionNote

When -show Option is not Specified

1

Option information

Option strings specified by a command line or subcommand

-

Output

2

Error information

Error messages

-

Output

3

Library information

Library information

-

Output

4

Information of modules, sections, and symbols within library

Module within the library

-

Output

When show=symbol is specified:
List of symbol names in a module within the library

-show=symbol

Not output

When show=section is specified:
Lists of section names and symbol names in a module within the library

-show=section

Not output

Note

All options are valid when the -list option is specified.