|
|
|
|
|
Macro
|
int_least8_t
uint_least8_t
int_least16_t
uint_least16_t
int_least32_t
uint_least32_t
int_least64_t
uint_least64_t
|
Indicates the types whose size is large enough to store signed and unsigned integer types of 8, 16, 32, and 64 bits.
|
|
int_fast8_t
uint_fast8_t
int_fast16_t
uint_fast16_t
int_fast32_t
uint_fast32_t
int_fast64_t
uint_fast64_t
|
Indicates the types which can operate signed and unsigned integer types of 8, 16, 32, and 64 bits at the fastest speed.
|
|
intptr_t
uintptr_t
|
These indicate signed and unsigned integer types that can be converted to or from pointers to void.
|
|
intmax_t
uintmax_t
|
These indicate signed and unsigned integer types that can represent all signed and unsigned integer types.
|
|
intN_t
uintN_t
|
These indicate N-bit signed and unsigned inter types.
|
|
INTN_MIN
INTN_MAX
UINTN_MAX
|
Indicates the minimum value of exact-width signed integer type.
Indicates the maximum value of exact-width signed integer type.
Indicates the maximum value of exact-width unsigned integer type.
|
|
INT_LEASTN_MIN
INT_LEASTN_MAX
UINT_LEASTN_MAX
|
Indicates the minimum value of minimum-width signed integer type.
Indicates the maximum value of minimum-width signed integer type.
Indicates the maximum value of minimum-width unsigned integer type.
|
|
INT_FASTN_MIN
INT_FASTN_MAX
UINT_FASTN_MAX
|
Indicates the minimum value of fastest minimum-width signed integer type.
Indicates the maximum value of fastest minimum-width signed integer type.
Indicates the maximum value of fastest minimum-width unsigned integer type.
|
|
INTPTR_MIN
INTPTR_MAX
UINTPTR_MAX
|
Indicates the minimum value of pointer-holding signed integer type.
Indicates the maximum value of pointer-holding signed integer type.
Indicates the maximum value of pointer-holding unsigned integer type.
|
|
INTMAX_MIN
INTMAX_MAX
UINTMAX_MAX
|
Indicates the minimum value of greatest-width signed integer type.
Indicates the maximum value of greatest-width signed integer type.
Indicates the maximum value of greatest-width unsigned integer type.
|
|
PTRDIFF_MIN
PTRDIFF_MAX
|
65535
+65535
|
|
SIG_ATOMIC_MIN
SIG_ATOMIC_MAX
|
127
+127
|
|
SIZE_MAX
|
65535
|
|
Macro
|
WCHAR_MIN
WCHAR_MAX
|
0
65535U
|
|
WINT_MIN
WINT_MAX
|
0
4294967295U
|
|
Function
(macro)
|
INTN_C
UINTN_C
|
Expanded to an integer constant expression corresponding to Int_leastN_t.
Expanded to an integer constant expression corresponding to Uint_leastN_t.
|
|
INT_MAX_C
UINT_MAX_C
|
Expanded to an integer constant expression with type intmax_t.
Expanded to an integer constant expression with type uintmax_t.
|