Print Address Range Settings dialog box


This dialog box is used to specify the address range to print the contents of the Disassemble panel.

Figure A.44

Print Address Range Settings Dialog Box

 

This section describes the following.

[How to open]

-

On the Disassemble panel, select [Print...] from the [File] menu.

[Description of each area]

(1)

Range specification area

Select a range to print from the following option buttons.

(a)

[Current display area] (default)

Prints only the contents of the Disassemble panel currently being displayed.

(b)

[Current selected area]

Prints only the range currently being selected in the Disassemble panel.

Note, however, that this option button will be disabled when nothing is selected in the Disassemble panel.

(c)

[Range of specified]

Specify the range of address to print via [Start address] and [End address]. You can either type address expressions directly into the text boxes (up to 1024 characters), or select them from the input history via the drop-down list (up to 10 items).

Remark

A symbol name at the current caret position can be complemented by pressing the [Ctrl] + [Space] key in each text box (see "2.19.2 Symbol name completion function").

[Function buttons]

Button

Function

OK

Closes this dialog box and opens the Windows dialog box to print the contents of the specified range of the Disassemble panel.

Cancel

Cancels the range specification and closes this dialog box.

Help

Displays the help for this dialog box.