2.17.2 Display only particular event types

Click on the toolbar button to display only the particular event type.

 

Displays events related to the Hardware Break.

 

[Full-spec emulator][E1][E20]

Displays events related to the Software Break.

 

Displays events related to the trace.

 

Displays events related to the timer.

 

[Full-spec emulator][E1][E20]

Displays events related to the performance.

 

Displays events related to the action event (Printf event).

 

Displays the built-in events (Unconditional Trace event and Run-Break Timer event).