2.7.1 Switching between cores (PEs)

The core (PE) to be debugged can be selected in either of the following two ways.

(1)

Switching through the statusbar

Select a desired PE from the drop-down list (shown below) on the statusbar in the Main window.

Figure 2.77

Statusbar on Main Window

(2)

Switching through the Debug Manager panel

Select a desired PE on the Debug Manager panel that are opened by selecting [Debug Manager] from the [View] menu.

Figure 2.78

Debug Manager Panel