2.10.3.3 Change display format of values

The display format of the [value] area can be changed using buttons below on the toolbar.

Notation

The following buttons to change the notation of a data value are displayed.

 

Hexadecimal

Displays the value of the selected item in hexadecimal number (default).

Signed Decimal

Displays the value of the selected item in signed decimal number.

Unsigned Decimal

Displays the value of the selected item in unsigned decimal number.

Octal

Displays the value of the selected item in octal number.

Binary

Displays the value of the selected item in binary number.

ASCII

Displays the value of the selected item in ASCII code.

 

Adds the value in hexadecimal number enclosing with "()" at the end of the value of the selected item.