2.8.3 Stop the program at the arbitrary position (breakpoint)

The program in execution can be stopped at the arbitrary position by setting a breakpoint. A breakpoint can be set by one-clicking with the mouse.

You need to configure the type of breakpoints to use before setting a breakpoint.

This section describes the following operations.

 

2.8.3.1 Set a breakpoint

2.8.3.2 Edit a breakpoint

2.8.3.3 Delete a breakpoint