To delete a break event (execution type) you have set, click the event mark displayed in the Editor panel/Disassemble panel.
Also, there is another way to delete a set break event. Select a Software Break event/Hardware Break event, or Combination Break event [E1][E20] in the Events panel, and then click the
button in the toolbar (see "2.15.5 Delete events").
In the Events panel, you cannot delete a break event (execution type) selectively in the combination breaks. All the break events (including access type) displayed in the detailed information on the combination break will be deleted. |