2.16.1.3 Check the output result

The following figure shows how the value of the specified variable expression is output to the [Debug Tool] tab of the Output panel (see Figure A.46 Output Result Format of Printf Event).

Figure 2.167

Example of Output Result of Printf Event