2.14.2.1 Checking the status bar for confirmation

When a program has stopped running, the measurement result is displayed in the status bar on the Main window (While no measurements are made, this status shows "Not measured").

Remark

When the EZ Emulator is in use, the status shown in the status bar is always "Not measured" because the EZ Emulator does not support the Run-Break timer function.

Figure 2.151

Example of a Run-Break Timer Event Measurement Result (Status Bar)