2.12.1 Display call stack information

Use the Call Stack panel shown below to display call stack information.

Select [Call Stack] from the [View] menu.

For details on the contents and function in each area, see the section for the Call Stack panel.

Caution

This panel is left blank while the program is in execution.
The contents of each area on this panel are displayed at the time the program has stopped running.

Figure 2.135

Displaying the Call Stack Information (Call Stack Panel)

 

This section describes the following.

 

2.12.1.1 Changing the form in which values are displayed

2.12.1.2 Jumping to the source line

2.12.1.3 Displaying local variables

2.12.1.4 Saving the displayed contents of call stack information