2.6.2.1 Changing the display mode

You can change the display mode of the Disassemble panel by clicking the button (toggle) on the toolbar.

 

-

Mixed display mode

In this display mode (default), the disassembled text is displayed combined with the source text.

Figure 2.88

Mixed Display Mode (Disassemble Panel)

 

-

Disassemble display mode

In this display mode, the source text is hidden and only the disassembled text is displayed.

Figure 2.89

Disassemble Display Mode (Disassemble Panel)