This class creates conditions of a conditional timer.
[Type]
class TimerCondition:
StartAddress = ""
StartData = ""
StartTimerType = TimerType.Execution
EndAddress = ""
EndData = ""
EndTimerType = TimerType.Execution
|
[Variable]
|
|
|
|
StartAddress
|
Specify an address starting timer measurement.
Must be specified.
|
|
StartData
|
Specify a data condition (number) of an address starting timer measurement.
This specification is ignored if TimerType.Execution is specified for StartTimerType.
|
|
StartTimerType
|
Specify the type of timers which start timer measurement.
The types that can be specified are shown below.
|
|
|
|
|
TimerType.Execution
|
Start a timer at execution (default)
|
|
TimerType.Read
|
Start a timer at data read
|
|
TimerType.Write
|
Start a timer at data write
|
|
TimerType.Access
|
Start a timer at data access
|
|
EndAddress
|
Specify the type of timers which end timer measurement.
Must be specified.
|
|
EndData
|
Specify a data condition (number) of an address ending timer measurement.
This specification is ignored if TimerType.Execution is specified for EndTimerType.
|
|
EndTimerType
|
Specify the type of timers which end timer measurement.
The types that can be specified are shown below.
|
|
|
|
|
TimerType.Execution
|
End a timer at execution (default)
|
|
TimerType.Read
|
End a timer at data read
|
|
TimerType.Write
|
End a timer at data write
|
|
TimerType.Access
|
End a timer at data access
|
[Detailed description]
- | "TimerCondition" is in class format, and the condition of a conditional timer is set in the variable.
In order to create a condition of a conditional timer, create an instance, and set conditions for that instance. |
[Example of use]
>>>execute_timer = TimerCondition() ... Create instance
>>>execute_timer.StartAddress = "main"
>>>execute_timer.StartTimerType = TimerType.Execution
>>>execute_timer.EndAddress = "sub"
>>>execute_timer.EndTimerType = TimerType.Execution
>>>debugger.Timer.Set(execute_timer) ... Specify function in which to set the conditional timer in parameter
1
>>>
|