This class holds the parameters when a build completes.
[Type]
class BuildCompletedEventArgs:
Error = None
Cancelled = False
HasBuildError = False
HasBuildWarning = False
|
[Variable]
|
|
Error
|
When an exception occurs in the build, this holds the error contents (System.Exception).
|
Cancelled
|
This holds whether the build execution was canceled or not.
|
HasBuildError
|
This holds whether an error occurred in the build or not.
|
HasBuildWarning
|
This holds whether a warning occurred in the build or not.
|
[Detailed description]
- | BreakCompletedEventArgs is a class, and it is passed as the argument only when the build.BuildCompleted event is issued.
It is not therefore possible to generate an instance of this class.
|
[Example of use]
>>>def buildCompleted(sender, e):
... print "Error = {0}".format(e.Error)
... print "BuildError = " + e.HasBuildError.ToString()
... print "BuildWarning = " + e.HasBuildWarning.ToString()
... print "BuildCancelled = " + e.Cancelled.ToString()
...
>>>build.BuildCompleted += buildCompleted ... Event connection
>>>build.All(True)
Error = None
BuildError = False
BuildWarning = False
BuildCancelled = False
True
>>> ... When an exception occurs, displayed as follows
>>>build.All(True)
Error = System.Exception:An error occurred during build.(E0203001)
BuildError = False
BuildWarning = False
BuildCancelled = False
False
>>>
>>> ... When a build error occurs, displayed as follows
>>>build.All(True)
Error = None
BuildError = True
BuildWarning = False
BuildCancelled = False
False
>>>
|