debugger.XCoverage.GetCoverage
|
This function gets the coverage. [IECUBE][IECUBE2][Simulator]
[Specification format]
debugger.XCoverage.GetCoverage(funcName, progName = "", fileName = "")
|
[Argument(s)]
|
|
funcName
|
Specify the function name to retrieve coverage for.
|
progName
|
Specify the name of the load module containing the function.
If there is only one load module, then this can be omitted (default).
|
fileName
|
Specify the name of the file containing the function.
If it is a global function, then this can be omitted (default).
|
Caution | If two or more parameters are specified, then three parameters must be specified. |
[Return value]
Value without "%" (numeric value)
Remark | The results of function execution are displayed with a "%" sign added. |
[Detailed description]
- | This function gets coverage for the function specified by funcName. |
- | If there are multiple load modules, specify progName. |
- | In the case of a static function, specify fileName. |
Caution | When a load module name (progName) or file name (fileName) is specified, it needs to be enclosed in double quotation marks (" ") in some cases. See "CS+ Integrated Development Environment Users Manual: Debug Tool" for details. |
Example | When file name "C:\path\test.c" is specified |
Or
[Example of use]
>>>debugger.XCoverage.GetCoverage("TestInit", "C:/test/Test.out", "C:/test/Test.c")
81.50%
>>>
|