CS+ Update Manager window


This window displays the status of and controls the update function.

Figure A.2

CS+ Update Manager Window

 

The following items are explained here.

[How to open]

-

From the Windows [Start] menu, select [Programs] >> [Renesas Electronics CS+] >> [Update Manager].

Remark

In Windows 8 or Windows 8.1, click on [Update Manager] on the start screen.

-

In the Windows task tray, click the or balloon help (i).

-

From the CS+ [Help] menu, select [Check for Updates...].

-

From the Create Project dialog box of the CS+, click the [Update...] button.

[Description of each area]

(1)

Menu area

This area displays a menu for changing the appearance and settings of the main area. Select an item to perform the corresponding action.

All

Displays the updates.

Microcontroller Name

Displays the updates corresponding to that microcontroller.

(Displays up to five microcontrollers for which the specify microcontroller function was used, most recent first.)

Download and install

Downloads the selected updates, and after the downloads are complete, install them.

Download only

Downloads the selected updates only.

Review update history

Displays the update history.

Restore hidden updates

Displays the Restore hidden updates page.

Change settings

Displays the Update Manager Options dialog box.

Help

Displays help.

Exit

Exits Update Manager.

(2)

Main area

Switch the display to one of the following pages, in accordance with the active function.